CyberPower Introduces Energy-Saving Green UPS

GreenPower UPS™ Technology Reduces UPS Energy Costs and Equipment

Date: March 21, 2008

SHAKOPEE, Minn., Feb. 22, 2008 – The past few years have seen rapid increases in energy prices as well as an increasing environmental awareness by consumers. For these reasons, CyberPower Systems has developed an uninterruptible power supply (UPS) technology that reduces energy consumption – GreenPower UPS™ technology. CyberPower is committed to leading the UPS industry in Green UPS designs that reduce energy consumption.

 After a year in development and hundreds of tests, the CyberPower engineering team zeroed in on an advanced-circuitry bypass design. The meticulously engineered design improves energy efficiency by significantly reducing energy consumption during normal utility power operation.

 “The patented GreenPower UPS™ design reduces the power consumption of UPS systems by up to 75% compared to conventional UPS systems,” said President of Manufacturing, Michael Ho.
 

The GreenPower UPS™ advanced-circuitry design is both impressive and solid. During normal power mode the GreenPower UPS™ design bypasses the Automatic Voltage Regulation (AVR) and Transformer. This patented technology dramatically reduces the energy used and heat generated by the transformer during normal mode. “Our competitors’ UPS systems have a significantly lower level of energy-efficiency. Especially when the UPS design is conventional online double-conversion, or line interactive and running under full load,” said Mr. Ho.

 How significant is GreenPower UPS™ technology? In a world where conserving the environment is an increasing concern energy-saving is not only a matter of cost-savings, but social responsibility. According to the 2007 Frost and Sullivan UPS Industry report, several million UPS units under- 5kVA UPS are sold in North America at a value of $1.6 billion. Consequently, “The cumulative cost-savings to customers, energy-savings, and reduction in environmental impact is truly remarkable,” said Director of Marketing, Brad Canham. Also, with an ability to reduce a UPS unit’s energy consumption by up to 75%, the energy-saved by individual and business users of GreenPower UPS™ technology is significant.

In turn, CyberPower channel partners are excited by the added-value of the energy savings that GreenPower UPS™ brings.  “An energy-efficiency design has become one of the top factors customers are considering when comparing UPS products,” said Director of VAR Channel Development, Pete Miesen.

 “There is no point to customer’s wasting energy and money on inefficient UPS systems when they don’t have to,” said VP of Worldwide Sales, Dan Ayala. “CyberPower is offering the best choice to customers who want an energy-efficient, reliable, meticulously engineered UPS.” 

GreenPower UPS™ Compliant UPS Systems

AVR Compact UPS Systems

Model VA/Watt Outlets
CP825AVRLCD 825/450 8

 

  AVR Tower UPS Systems

Model VA/Watt Outlets
CP900AVR 900/560 8
CP1200AVR 1200/720 8
CP1500AVRT 1500/900 8

 

Intelligent AVR Tower LCD UPS Systems

Model VA/Watt Outlets
CP850AVRLCD 850/510 9
CP1000AVRLCD 1000/600 9

 

Intelligent AVR Tower LCD UPS Systems

Model VA / Watts Outlets
CP1285AVRLCD 1285/750 8
CP1350AVRLCD 1350/810 8
CP1500AVRLCD 1500/900 8

 

Smart App 1U Rackmount LCD UPS Systems 

Model VA / Watts Outlets
OR500LCDRM1U 500/300 6
OR700LCDRM1U 700/400 6
OR1000LCDRM1U 1000/700 6
OR1500LCDRM1U 1500/900 6

 

Smart App 2U Rack/Tower LCD UPS Systems

Model VA / Watts Outlets
OR1500LCDRM2U 1500/900 8
OR2200LCDRM2U 2000/1320 8

 

Smart App Sinewave LCD UPS Systems

Model VA / Watts Outlets
PR750LCDRM1U 750/560 6
PR1000LCDRM1U 1000/750 6
PR1000LCDRT2U 1000/700 8
PR1000LCDRTXL2U 1000/700 6
PR1500LCDRT2U 1500/1000 8
PR2200LCDRT2U 2170/1600 8