CyberPower Systems Introduces Industrial-Grade Power Distribution Units
New PDU lineup includes more than 80 Basic, Metered and Switched models designed for maximum reliability and flexibility for high-density applications.
Minneapolis, Minn. (April 21, 2010)—CyberPower Systems, the global leader of innovative power protection and distribution equipment, today announced the availability of the most comprehensive lineup of Power Distribution Units (PDUs) in the market space. Offering over 80 models, CyberPower’s PDU lineup includes Basic, Metered and Switched PDU models in horizontal and vertical rack-mount configurations, fulfilling the demand for versatile power distribution, especially in demanding, high-density environments.
“CyberPower is committed to providing data center customers a broad line up of PDU products that offer incredible flexibility, configurability and quality that is second to none.” stated Dan Ayala, CyberPower’s Vice President of Worldwide Sales. “Our comprehensive PDU offering provides countless configuration options and allows IT managers to make exact sizing decisions to help lower the total cost of ownership. Entering into this new category will bring us even closer to the needs of the customer in the data center space.”
All CyberPower PDUs offer industrial-grade durability and world-class reliability, backed by a lifetime warranty, ensuring years of dependable performance. The PDU configurations range from 8 to 38 outlets and include 15, 20 and 30-amp capacities with a circuit breaker. Every PDU offers industrial-grade metal housing, a flexible AC power cord, a cord retention tray and is ETL certified. CyberPower PDUs are designed and rigorously tested to distribute unfiltered electrical pass-through of conditioned power from a UPS or utility power from a wall outlet to multiple connected devices including networks, servers, workstations and telecom systems.
“The addition of our PDU products to our award-winning UPS systems helps to simplify the decision making process for our customers - saving time and money.” added Jonah Cagley, Director of Marketing at CyberPower.
CyberPower Basic PDUs provide unfiltered electrical pass-through in versatile 8 to 32-outlet configurations and are available in 1U rack and 0U vertical mounting options for demanding applications, requirements and environments.
CyberPower Metered PDUs provide unfiltered electrical-pass through in 8 to 32-outlet configurations, a front LCD panel displaying the connected equipment current draw for real-time load monitoring and are available in 1U rack and 0U vertical mounting options that provide maximum flexibility for high-density applications and environments.
CyberPower Switched PDUs provide unfiltered electrical-pass through in 8-outlet configurations, a front LCD panel displaying the connected equipment current draw for real-time load monitoring, available in 1U rack and 0U vertical mounting options for maximum configuration flexibility and include a network interface allowing remote load access and management, as well as control of individual outlets. Additionally, Switched PDUs are UL1419 and FCC Class B certified.
All CyberPower PDUs are 100% RoHS compliant. RoHS aims to improve environmental conditions worldwide by strictly limiting the use of six hazardous substances: lead, mercury, cadmium, hexavalent chromium, polybrominated biphenyls (PBBs) and polybrominated diphenyl ether (PBDE). CyberPower manufactures an extensive line of environmentally-friendly, RoHS-compliant power protection products.
For more information on CyberPower’s Power Distribution Units, visit: www.cpsww.com/pdus
About CyberPower Systems, Inc.
CyberPower Systems, Inc. designs and manufactures state-of-the-art power protection and distribution equipment for corporate, business, home, government and educational markets. CyberPower leads the industry by surpassing customer expectations in the development, design, construction, durability and functionality of uninterruptible power supply (UPS) products for computers, peripherals and connected devices. CyberPower Systems operates in the Asian Pacific, North American, and European markets. For additional information, including sales office locations and authorized reseller partners, visit cpsww.com.
Media Contact
Jonah Cagley
Director of Marketing
Phone: +1 (952) 567-7943
CyberPower Systems (USA), Inc.
4241 12th Avenue East, Suite 400
Shakopee , MN 55379
Phone: +1 952-403-9500
Fax: 952-403-0009
E-mail: sales@cyberpowersystems.com
United States