OR LCD Series FAQs
How to rotate the LCD:
1 Locate the small notches on either side of the square display.

2 Insert a small screwdriver into the notch and gently pry up the square display. Switch back and forth prying one side then the other to gently work it out far enough that you can grasp it with your fingers and pull it out.
3 Once it is out rotate it to the preferred orientation and push it back in.
United States