Advisory Notices

ATS PDU Mainboard Firmware v1.06

Firmware Version 1.06 Notes  | Priority: Critical

Date: August 10, 2017      Filename: cpsatsmafw_106.bin

 

Version 1.06 is a critical, functional release. It contains a bug fix where under specific circumstances the transfer time between the input power sources, during a power loss of either source, results in discontinuity of power supplied through the ATS PDU. It is recommended that the ATS PDU Mainboard firmware update be installed as soon as possible to prevent a potential power loss when switching between the A and B power sources.

In addition to this firmware update, it is recommended that when one ATS PDU source is connected to a UPS system and the second source is connected to another power supply (generator, utility, other) the preferred source setting on the ATS PDU should be set to the UPS power source.

Download ATS PDU Mainboard Firmware v1.06

Download ATS PDU Firmware Upgrade Instructions

 

Applicable Product Series:

  • Metered Auto Transfer Switch (ATS) Power Distribution Unit (PDU)
  • Switched Auto Transfer Switch (ATS) Power Distribution Unit (PDU)

 

Applicable Products:

  • PDU30MT17AT
  • PDU20SWT17ATNET
  • PDU15SWHVIEC12ATNET
  • PDU30SWHVT19ATNET
  • PDU30SWT17ATNET
  • PDU15SW10ATNET
  • PDU15MHVIEC12AT
  • PDU20SWT10ATNET
  • PDU20SW10ATNET
  • PDU20M10AT
  • PDU20MT10AT
  • PDU20SWHVT10ATNET
  • PDU20SWHVIEC10ATNET
  • PDU30MHVT19AT
  • PDU20MHVT10AT
  • PDU20MHVIEC10AT
  • PDU15M10AT

For questions, please contact tech support at 877.297.6937 or tech@cpsww.com.