Latest generation of best-selling product line offers enhanced features for ease of use and power management
SHAKOPEE, Minn. – Cyber Power Systems (USA), Inc. a leader in power protection and power management products, announced the release of its latest generation of PFC Sinewave Mini-Tower UPS (uninterruptible power supply) Systems providing surge protection and sine wave battery backup. The UPS systems are suited for home and office use, including desktop PCs, Mac computers, home entertainment equipment, gaming systems, and other ENERGY STAR® electronics which require active PFC (power factor correction) source compatibility. The utility-grade, sine wave battery output delivers the highest level of power quality for high-end equipment.
“The CyberPower PFC Sinewave Mini-Tower UPS Systems have been redesigned from the ground up to make a popular product line even better,” said Tracey McMeekin, senior product manager at CyberPower. “We’ve added customer-inspired features for greater ease of use and more flexible at-a-glance management.”
Best-selling UPS systems
The CyberPower PFC Sinewave Mini-Tower product family is one of the best-selling lines of UPS systems in North America. The new CyberPower PFC Mini-Tower series includes four models—CP850PFCLCD, CP1000PFCLCD, CP1350PFCLCD and CP1500PFCLCD—with outputs ranging from 850 VA/510 Watts to 1500 VA/1000 Watts. Features of the new CyberPower line include:
- Sine wave output powers sensitive electronics during outages when in battery mode, keeping critical equipment running smoothly during power interruptions.
- Redesigned multi-function, color LCD control panel provides at-a-glance alerts of working status and potential power problems.
- Panel screen tilts up to 22 degrees for easy viewing when the UPS is placed in lower positions.
- USB-C and USB-A charging ports allow charging of personal devices such as mobile phones and tablets, even during a power failure.
- Remote monitoring and management of the UPS with optional RMCARD205 (1500 VA model only).
- Watch our feature video
Like all CyberPower professional-grade power protection products, the PFC Sinewave Mini-Tower UPS Systems are compatible with CyberPower’s PowerPanel® power management software. PowerPanel is available for free download at https://www.cyberpowersystems.com/products/software/.
About Cyber Power Systems (USA), Inc.
CyberPower designs and manufactures uninterruptible power supply systems, power distribution units, surge protectors, remote management hardware, power management software, mobile chargers, and connectivity products. The company serves customers in enterprise, corporate, government, education, healthcare, and small office/home office environments. CyberPower products are available through authorized distributors and sold by value-added resellers, system integrators, managed service providers, select retailers, and online resellers. For more information, visit:
https://www.cyberpowersystems.com/.
Cyber Power Systems (USA), Inc.
Tim Madsen, 952-403-9500
tmadsen@cpsww.com