Scalable, enhanced cloud software for remote monitoring and management of CyberPower and third-party devices
SHAKOPEE, Minn. – Cyber Power Systems (USA), Inc. a leader in power protection and power management products, announced today the launch of PowerPanel® Cloud Pro and PowerPanel® Gateway software, expanding its offering of remote monitoring to an unlimited number of UPS (uninterruptible power supply) systems and power distribution units (PDUs) from anywhere there is an internet connection. PowerPanel Gateway introduces the ability to cloud-monitor legacy connected devices. The solutions offer enhanced functionality to reduce IT resources and improve operating efficiencies.
Designed for use by managed service providers (MSPs), decentralized service providers and IT professionals, the CyberPower PowerPanel Cloud Pro and the PowerPanel Gateway solutions are designed to serve SMB and enterprise-level organizations with 20 or more employees.
PowerPanel Cloud Pro
CyberPower Power Panel Cloud Pro is packed with all the functionality of the innovative PowerPanel® Cloud software, which CyberPower premiered in 2021, but offers additional features for greater convenience and flexibility.
PowerPanel Cloud Pro is completely scalable, expanding the available IoT connections to an unlimited number of CyberPower and third-party UPS systems—suited for MSPs who need to monitor multiple locations or clients on same platform.
Tim Derochie, director of applications engineering at CyberPower, said: “We specifically developed Cloud Pro for the MSP channel as a convenient way to manage devices on a scalable, flexible basis. This feature set has proven to be popular with SMB to enterprise customers.”
- Users only pay for what they use: partners have flexible billing options, including monthly billing and upfront purchasing to streamline node acquisition. It provides companies with the ability to add and remove devices as needed with charges for actual usage versus a fixed amount of annual nodes.
- Multi-user access with admin and user permissions to manage access rights: groups or subgroups within a company can be monitored separately in a hierarchical view or by permission levels across different locations locally, nationally or globally.
- Single Sign-On (SSO) authentication: improves security and reduces the time users spend signing in.
PowerPanel Cloud Gateway
The CyberPower PowerPanel Cloud Gateway, available as a free download, offers the convenience of adding connected devices to a PowerPanel Cloud account. This feature enables MSPs and IT managers to remotely monitor connected legacy CyberPower devices and third-party UPS systems in the cloud.
Derochie said: “For users of PowerPanel Cloud Pro, our new cloud gateway bypasses the need for additional hardware. Essentially, the PowerPanel Cloud Gateway allows users the ability to connect CyberPower and third-party UPS to the cloud without installing cloud cards.”
- Supports all CyberPower UPS, PDU, and ATS (automatic transfer switch) devices as well as third-party UPS systems that use the CyberPower MIB key, allowing users to monitor their equipment anytime, anywhere.
- Easily add devices to both PowerPanel Cloud and PowerPanel Cloud Pro software.
- Through PowerPanel Cloud Gateway, multiple device ecosystems may be connected to a user’s PowerPanel Cloud account so they can monitor devices across multiple networks or multiple locations.
About Cyber Power Systems (USA), Inc.
CyberPower designs and manufactures uninterruptible power supply systems, power distribution units, surge protectors, remote management hardware, power management software, mobile chargers and connectivity products. The company serves customers in enterprise, corporate, government, education, healthcare and small office/home office environments. CyberPower products are available through authorized distributors and sold by value-added resellers, system integrators, managed service providers, select retailers, and online resellers. For more information, visit: https://www.cyberpowersystems.com/.
Contacts
Cyber Power Systems (USA), Inc.
Tim Madsen, 952-403-9500
tim.madsen@cyberpower.com