![](https://dl4jz3rbrsfum.cloudfront.net/images/feature-focus/7034_cpu_web_featurefocus_imagefix.jpg)
Power Device Network Utility
The Power Device Network Utility gives users an easy-to-use interface for establishing the IP addresses of CyberPower PDU devices, RM Cards, and PowerPanel Business Edition Agents and Clients. It scans network devices with MAC addresses that match CyberPower network hardware. Once found, the device(s) can then be configured with a specific IP address, subnet mask, and gateway address, allowing the device(s) to work properly on the network and to integrate with the CyberPower Management Console.