Wirecutter Selects CP900AVR as Best Uninterruptible Power Supply (UPS)

May 8, 2024 by CyberPower

Wirecutter, an online product recommendation website from the New York Times, recently named the CyberPower CP900AVR UPS System as the best UPS for a home network in 2024.

Wirecutter cited the model’s runtime, ease-of-use, and compact size. The model was also recognized as an ideal battery backup solution for most people during common power outages.

The CyberPower CP900AVR UPS review also highlighted its premium features commonly found in battery backup solutions costing twice as much. Among these features was automatic voltage regulation (AVR) that provides more reliable power to connected devices that are unable to tolerate power drops and extends the overall life of the unit.

Wirecutter’s evaluations were based on feature set, in-house performance testing, warranty terms, and overall design.

Read the full article here.

About Wirecutter

Wirecutter was founded in September 2011 and acquired by The New York Times in October 2016. Wirecutter strives to be the most trusted product recommendation service around and works with total editorial independence. They don’t post a recommendation unless their writers and editors have deemed something the best through rigorous reporting and testing.