Cyber Power Systems (USA), Inc. a leader in power protection and power management products, today announced that Game Rant, a digital publication for gaming enthusiasts, has named three of its UPS (uninterruptible power supply) systems as top battery backup units for gaming.
“We are excited to be recognized by Game Rant for our UPS systems that help gamers protect their gear and extend game time during power events and outages,” said Brent Lovett, general manager and president of CyberPower. “Notably, all three of the high-rated CyberPower UPS systems for gaming feature active PFC (power factor correction) power source compatibility and sine wave output to power and protect advanced electronic equipment.”
Here’s a look at Game Rant’s top picks:
A CyberPower bestseller suitable for many types of electronics and applications, Game Rant deemed the PFC Sinewave CP1500PFCLCD battery backup system as Best Overall UPS for Gaming. With a 1500VA power capacity, the system provides a sufficient amount of run time during power outages, and includes 12 outlets and two USB charging ports.
Named Best High-End UPS for Gaming, the CyberPower PFC Sinewave OR2200PFCRT2U battery backup system features a robust 2200VA of power capacity to address power disruptions and outages affecting the most demanding of gaming systems. The UPS system also offers versatility in a rack/tower convertible form factor and eight outlets.
Lastly, Game Rant named the CyberPower PFC Sinewave CP1000PFCLCD battery backup system the Best UPS for Console Gaming, making it ideal to support PlayStation 5, Xbox Series X/S and other gaming consoles. With a 1000VA rating and a mini-tower tower form factor, the compact unit is outfitted with 10 outlets and two USB charging ports.
Read the full CyberPower UPS reviews at GameRant.com.
About Cyber Power Systems (USA), Inc.
CyberPower designs and manufactures uninterruptible power supply systems, power distribution units, surge protectors, remote management hardware, power management software, mobile chargers and connectivity products. The company serves customers in enterprise, corporate, government, education, healthcare and small office/home office environments. CyberPower products are available through authorized distributors and sold by value-added resellers, system integrators, managed service providers, select retailers, and online resellers. For more information, visit:
https://www.cyberpowersystems.com/.
About Game Rant
Founded in 2009 and acquired by Valnet Inc. in 2019, Game Rant is a digital publication run by gamers with articles written for gamers with an emphasis on news, reviews, unique features and interviews. We aim to tap into the topics and subjects that Game Rant, as gamers, are most passionate about. Game Rant is a top three Comscore games media publisher by total monthly views, with more than 110 million monthly page views and over 87 million monthly sessions. For more information, visit https://gamerant.com.
Contacts
Cyber Power Systems (USA), Inc.
Tim Madsen, 952-403-9500
tim.madsen@cyberpower.com