What is Firewire?

FAQ Category:

Firewire or FireWire® Cable is also known as IEEE 1394. The original release of IEEE 1394-1995 is now known as Firewire 400. It can transfer data between devices at 100, 200, or 400 Mbit/s. The cable’s maximum length is limited to 14.8 ft. (4.5 meters), but you can have up to 16 cables daisy-chained by using active repeaters, external hubs, or internal hubs.

TECHNICAL SUPPORT
Please contact our Tech Support department with installation, troubleshooting, or general product questions.
Hours of operation: Monday – Friday 7:00am – 6:00pm CST
Contact Tech Support: Submit Ticket Now
  • Was this Helpful ?
  • Yes   No